{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to have two modules connected to one M340 NOE Ethernet module, or two NOE each with a TCSEGPA23F14F gateway?

Issue

Is it possible to have two modules connected to one M340 NOE Ethernet module, or two NOE each with a TCSEGPA23F14F gateway?

Product Line

Modicon M340

Environment

BMXNOE0100, TCSEGPA23F14F

Resolution

You can have several Modbus TCP IO scanners in the same PLC, each of them supporting several PRMs. This limit depends on the PLC type.
You can plug several PRM on the same I/O scanner module as long as the I/O scanner limit of 2KW in and 2KW out is not exceeded.

Schneider Electric Saudi Arabia