{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the difference between Set and Force to 0 and 1 using Unity Pro?

Issue:
Difference between Set and Force to 0 and 1 using Unity Pro


Product Line:
Unity Pro/EcoStruxure Control Expert


Resolution:
The Set to 0 and Set to 1 under the Services menu is used to modify the value of a BOOL or EBOOL located or unlocated variables to 1 or 0.  The value can be overwritten in logic.  The Force to 0 and Force to 1 can only be used to force the value of a located EBOOL to 0 and 1.  The value cannot be overwritten in the logic.


Schneider Electric Saudi Arabia