Goals and Symptoms
If an XBTP application has been converted to be downloaded into XBTPM device. Only 8 lines will be displayed and noway to scroll the lines from 8 upto 25
Facts and Changes
XBTL1000 V4.42 XBTP et XBTPM
Causes and Fixes
4 HOW TO CONVERT THE XBT-P APPLICATION TO XBT-PM ?
2 possibilities must be assessed:
1. XBT-P has no printer port
In that case, the XBT-P can be substituted either by a XBT-PM027010 or by a XBT-PM027110.
This is the procedure to follow:
a. Convert the XBT-P application to one of the following PRODUCTS:
- XBT-E013010
- XBT-E014010
- XBT-E015010
- XBT-E016010
- XBT-E013110
- XBT-E014110
- XBT-E015110
- XBT-E016110
b. Transfer the XBT-E application to the XBT-PM027010 or to the XBT-PM027110.
2. XBT-P has printer port
In that case, the XBT-P is substituted by a XBT-PM027110
This is the procedure to follow:
a. Convert the XBT-P application to one of the following PRODUCTS:
- XBT-E013110
- XBT-E014110
- XBT-E015110
- XBT-E016110
b. Transfer the XBT-E application to the XBT-PM027110.
Plus:
The scrolling is possible on XBT-PM hardware using a XBT-E application.
All the static function keys are converted (12 function keys maximum on XBT-P and on XBT-PM)
All alarm, application and form pages are converted.
All the functions of the dialogue table are converted.
Minus:
As the application is in fact a XBT-E application, no graphical objects (bar graphs, gage variable field) and no background picture can be added on the XBT-PM display.
No dynamic function keys are available also in these conditions.
But these features were not possible on XTB-P.
Legacy KB System (APS) Data: RESL180743 V1.0, Originally authored by on , Last Edited by JaOu on 12/04/2006
Related ranges: XBT L1000
Released for:Schneider Electric Saudi Arabia