{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
It appears that communications is intermittent and the unit is not responding appropriately.

Possible problem and solution:

The VW3L3P01R40 cable has a five-volt DC input, which should be used if intermittent or no communication is encountered.
Use a 5 VDC regulated power supply with at least 50 mA current.
The power jack is for a 2.5 mm diameter plug center polarized connector.

Be sure to check the baud rate set in Lexum CT, and be sure it is the same as the Lexium ILP/ILT baud rate setting.


Legacy KB System (APS) Data: RESL200114 V1.0, Originally authored by MaPr on 09/28/2009, Last Edited by MaPr on 09/28/2009
Related ranges: Lexium ILT, ILP

Schneider Electric Saudi Arabia