{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Lexium32 encoder connector plugs (type/specification and tools) used on the amplifier end of the encoder cable ?

Goals and Symptoms

Lexium32 encoder connector plugs (type/specification and tools)
used on the amplifier end of the encoder cable ?

Causes and Fixes

We use with our encoder cables:

Y-ConPlug-31 (Plug) and Y-ConIP20Lock-10
(IP20-Strain relief with vibration resistant locking clips),

The tools reqired for cable assembly can be ordererd directly
from the manufacturer:

Crimping tool for encoder connector RJ45 10 pins:
Yamaichi Y-Con Tool-11, Y-Con Tool-20, Y-Con Tool-30
( www.yamaichi.com )

Crimping tool for encoder connector M23:
Coninvers SF-Z0007 ( www.coninvers.com )

Crimping tool for power connector M23/M40:
Coninvers SF-Z0008 ( www.coninvers.com )

Please look to the attached catalogues for connector and tools

Attachments

(Removed File URL: 201460_E336/RJ45.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/f86ffec6312f0352c12576d6004219c3/fl_block_5/0.60E?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL201460 V1.0, Originally authored by BeBr on 02/26/2010, Last Edited by BeBr on 02/26/2010
Related ranges: Lexium 32

Schneider Electric Saudi Arabia

Attachment(s)

RJ45.zipRJ45.zip [378.07 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: