{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to use the sin-ramp type in a LMC20 CNC-application?

Goals and Symptoms

How to use the sin-ramp type in a LMC20 CNC-application?

Causes and Fixes

The ramp-type settings in the drive-configuration works only for single axis movements (for example MC_MoveAbsolute,....). For CNC-application (Using of SMC_Interpolator and SMC_ControlAxisByPos, the input "iVelMode" of the Interpolator needs to set to "1". Different jerk values are not possible.


Legacy KB System (APS) Data: RESL202091 V1.0, Originally authored by JoAr on 04/23/2010, Last Edited by JoAr on 04/23/2010
Related ranges: Lexium Controller LMC10 - LMC20

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: