{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Will Dynamic Host Configuration Protocol (DHCP) requests pass through a router?

DHCP requests sent by the client device, or client computer are broadcasts. Routers do not pass broadcasts through to other networks. This prevents a broadcast problem on one network from propagating to another. To use DHCP across a routed network, a DHCP/ BOOTP relay agent must be employed (RFC 1542). ( DHCP is an extension of the bootstrap protocol (BOOTP), refer to RFC 951).
A relay agent is a program used to pass specific types of IP packets between subnets. A DHCP/BOOTP relay agent simply passes DHCP/BOOTP messages (IP packets) from one subnet to another. It can be software or hardware based. Some routers are RFC 1542-compliant. These have an agent built in to them.


Legacy KB System (APS) Data: RESL1205 V1.0, Originally authored by on , Last Edited by on
Related ranges: ConneXium - Ethernet

Schneider Electric Saudi Arabia