Goals and Symptoms
There are 6 motors with below power: 110 , 132, 160, 200, 200,160 kW Is it possible to start them with a single soft starter.
Facts and Changes
cascading
Causes and Fixes
The best way is to use a soft starter ( ATS48 ) for this kind of application with cascading sequence ( see user manual )
Legacy KB System (APS) Data: RESL156437 V3.0, Originally authored by on , Last Edited by on
Related ranges: Altistart 48
Released for:Schneider Electric Saudi Arabia