{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Momentum M1E 984LL Exec. Upgrade to v.1.20

Issue
The purpose of this resolution is to inform Momentum product users that the M1E 984LL Executive firmware for the M1E processors has been upgraded to v.1.20. The SV has changed from 1.08 to 1.20.

'M1E I/O Status' web page is misleading. A single generic Momentum I/O base displays the same LED pattern for the various modules available. These LED's only show the first I/O mapped input and output word, regardless if its an analog module or a discrete base.

  1. Web page applets not displayed. Web page applets could not be displayed in a browser only if the web pages were downloaded to the M1E using the Web Loader Utility on a Win98 Operating System.
  2. Classfull addressing.


Product Line
Momentum
170CCC96020
170CCC96030
170CCC98020
170CCC98030



Environment


Resolution
Update to firmware v.1.20.

The M1E I/O Status web page has been changed to the I/O and Register Data Display. This new page allows the user to enter a 3x or 4x register into the first location of a table of 15 continuous registers to view the value in those registers.
  1. Fixes a problem displaying web page applets only if the web pages were downloaded to the M1E using the Web Loader Utility on a Win98 Operating System.
  2. Supports Classless addressing.

Schneider Electric Saudi Arabia