{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

To identify the voltage limits or Tolerence for the ZB4-BW0** transformer pilot light bodies? Can the ZB4BW055 operate upto 440V?

Goals and Symptoms

To identify the voltage limits or Tolerence for the ZB4-BW0** transformer pilot light bodies? Can the ZB4BW055 operate upto 440V?

Facts and Changes

ZB4
ZB4BW
Transformer
Voltage Limits

Causes and Fixes

The voltage limit is +/- 10%.
=> Mini = 360V~ - Maxi = 440V~.


Legacy KB System (APS) Data: RESL160826 V1.0, Originally authored by LaBe on 09/19/2007, Last Edited by LaBe on 09/19/2007
Related ranges: Harmony style 4

Schneider Electric Saudi Arabia