{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does service release 8 for ProWORX NxT v2.20 include all the service releases from one through eight?

Issue

Does service release 8 for ProWORX NxT v2.20 include all the service releases from one through eight?

Product Line

ProWorx

Environment

ProWorx NxT v2.20

Resolution

ProWORX NxT v2.20 service release 8 does not include all the service releases. It only includes service release 8. You must have ProWORX NxT v2.20 service release 6A, which includes service releases one through six, installed prior to installing service release 8. There is no public release of service release 7.

Schneider Electric Saudi Arabia