Search FAQs
Does the AS-BDEA-203 allow the TSX Compact controllers to act as a Profibus Master?
Issue
Does the AS-BDEA-203 allow the TSX Compact controllers to act as a Profibus Master?
Product Line
TSX Compact
Environment
AS-BDEA-203
Resolution
No. The AS-BDEA-203 module is a Profibus drop adapter. It allows a drop of Compact I/O to be controlled by a Profibus DP master. It cannot be used in conjunction with a Compact CPU and has no master capability.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: