{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can the 6000-021 Cybercalc software be run on Pentium based PCs?

Issue
Can the 6000-021 Cybercalc software be run on Pentium based PCs?

Product line
Cybercalc

Environment
6000-021

Resolution
The 6000-021 Cybercalc software is not qualified for usage on Pentium based PCs, however it has been used previously with success. You may need to run SLODOS, CPUKILLER, or other freeware to slow the PC down.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: