{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the difference between the SyMax 8030PS25/35 power supplies and the 8030PS25F/35F power supplies?

Issue
What is the differene between the SyMax 8030PS25/35 power supplies and the 8030PS25F/35F power supplies?

Product line
SY/MAX

Environment
8030PS25

Resolution
The PS25F and PS35F power supplies are identical in function to the PS25 and PS35 modules, except that they do not have an ON/OFF switch located on the front of the module. A separate main disconnect switch or circuit breaker must be installed to shut off power to the programmable controller system.


NOTE: The Sy/Max product line was obsoleted 12/31/2013 and the recommneded upgrade is the M580, contact your local distributor or SchneiderElectric for more information.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.