{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Solution Interval for the PCFL (KPID) function block is incorrectly defined as floating point.

issue
The solution interval for the PCFL( KPID) function block is incorrectly defined as a 'Floating Point' radix instead of the expected 'Long (32 Bit) Integer'.

Product Line
ProWORX 32, Concept

Environment
Windows 7

Resolution
Attempts to enter a floating point value will cause the block to return an error.

Download the attached 'PCFL.ZIP' file and extract the PCFL.UCS file to your ..\ProWORX\32\Scripts folder and replace the existing file with it.

Attachments

Schneider Electric Saudi Arabia

Attachment(s)
PCFL.zip [4.43 KB]