{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement for the 57-0089-000 (2A 250V slow blow) fuse?

Issue
Part number 57-0089-000 is no longer active sale. Need something to use in its place.

Product line
Modicon Quantum

Resolution
57-0089-000 corresponds to Littelfuse 326002, .25 x 1.25 ceramic.

https://www.littelfuse.com/~/media/electronics/datasheets/fuses/littelfuse_fuse_325_326_datasheet.pdf.pdf

Schneider Electric Saudi Arabia