{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Momentum M1E Ethernet Port Lockup Caution

Issue
The purpose of this resolution is to inform users of Momentum M1E Processor of a potential problem of the Ethernet port locking up under certain conditions.

The M1E Processor Ethernet port will lock up if the Constant Sweep function is enabled and the PLC scan time exceeds the user configured Constant Sweep time. This will occur regardless of which 984LL or IEC Exec is used. When the fault occurs, the unit will produce a stopped error code 80 and the user is not able to log back in and an error: "Illegal Modbus function code. Error Id: OL9-21581" will be displayed.


Product Line
Momentum
171CCC96020
171CCC98020
171CCC96030
171CCC98030


Resolution
This issue is under investigation by Engineering. An update to this Resolution will be made available when new information from engineering is received.

Recovery from this fault requires user intervention. To recover, power cycling alone will not clear the fault, but removing the battery and leaving the unit powered down for 5 minutes, will allow access through the Ethernet port once power is restored.

To avoid this issue, the constant sweep function in the PLC should be disabled.

Schneider Electric Saudi Arabia