To inform users the byte order of MBP_MSTR "Get Local Statistics" Board Status for different 140NOE77101/11 and 140NOE77100/10 versions and which order will be consistently used for future product releases.
Product Line
EcoStruxure Control Expert (former Unity Pro), Modicon Quantum
Environment
140NOE77101
Resolution
140NOE77111/01 V2.0, V3.0, V3.1, V3.3, V3.6 & 140NOE77100/10 V3.0, V3.3, V3.4 has the same order as the table below:
Bit # | Definition |
15 | 0=link LED off; 1= Link LED on |
14 | 0=Application LED off; 1= Application LED on |
13 | 0=twisted pair; 1=fiber |
12 | 0=10Mbit; 1=100Mbit |
11... 8 | Reserved |
7... 4 | Module Type |
3 | Reserved |
2 | 0=half duplex; 1=full duplex |
1 | 0=not configured; 1=configured |
0 | 0=PLC not running; 1=PLC/NOE running |
NOTE: Bit 0 is a low bit counting from right side, so that means: PLC Running = 0x0001, Application LED = 0x4000, LED connection = 0x8000.
140NOE77111/01 V3.5 & 140NOE77100/10 V1.02, V2.0 has the same order as the table below:
Bit # | Definition |
15...12 | Module Type |
11 | Reserved |
10 | 0=half duplex; 1=full duplex |
9 | 0=not configured; 1=configured |
8 | 0=PLC not running; 1=PLC/NOE running |
7 | 0=link LED off; 1= Link LED on |
6 | 0=Application LED off; 1= Application LED on |
5 | 0=twisted pair; 1=fiber |
4 | 0=10Mbit; 1=100Mbit |
3...0 | Reserved |
NOTE: Bit 0 is a low bit counting from right side, so that means: PLC Running = 0x0100, Application LED = 0x0040 , LED connection = 0x0080.
2. Documentation Mismatch:
· Unity V2.2 and Concept V2.2, V2.6 help file uses the same byte order as table 1.
· Modicon Quantum with Unity Ethernet Network Modules User Manual (6/2006) and Transparent Ready User Guide (10/2005) use the same byte order as table 2.
We have swapped MBP_MSTR Get local statistics Word3 board status byte order when we released certain firmware versions. This also causes the product user manual, and Unity, Concept Help file board status description mismatch issue.
Considering majority users have been using the order same as the current version V3.6 for NOE77111/01 and V3.4 for NOE77100/10, we decide to remain the current MSTR board status byte order (shown in table 1) for NOE module and will make sure the consistency in our future release.
Schneider will correct the corresponding documentation to reflect the change.
Released for: Schneider Electric Saudi Arabia
To inform users the byte order of MBP_MSTR "Get Local Statistics" Board Status for different 140NOE77101/11 and 140NOE77100/10 versions and which order will be consistently used for future product releases.
Product Line
EcoStruxure Control Expert (former Unity Pro), Modicon Quantum
Environment
140NOE77101
Resolution
140NOE77111/01 V2.0, V3.0, V3.1, V3.3, V3.6 & 140NOE77100/10 V3.0, V3.3, V3.4 has the same order as the table below:
Bit # | Definition |
15 | 0=link LED off; 1= Link LED on |
14 | 0=Application LED off; 1= Application LED on |
13 | 0=twisted pair; 1=fiber |
12 | 0=10Mbit; 1=100Mbit |
11... 8 | Reserved |
7... 4 | Module Type |
3 | Reserved |
2 | 0=half duplex; 1=full duplex |
1 | 0=not configured; 1=configured |
0 | 0=PLC not running; 1=PLC/NOE running |
NOTE: Bit 0 is a low bit counting from right side, so that means: PLC Running = 0x0001, Application LED = 0x4000, LED connection = 0x8000.
140NOE77111/01 V3.5 & 140NOE77100/10 V1.02, V2.0 has the same order as the table below:
Bit # | Definition |
15...12 | Module Type |
11 | Reserved |
10 | 0=half duplex; 1=full duplex |
9 | 0=not configured; 1=configured |
8 | 0=PLC not running; 1=PLC/NOE running |
7 | 0=link LED off; 1= Link LED on |
6 | 0=Application LED off; 1= Application LED on |
5 | 0=twisted pair; 1=fiber |
4 | 0=10Mbit; 1=100Mbit |
3...0 | Reserved |
NOTE: Bit 0 is a low bit counting from right side, so that means: PLC Running = 0x0100, Application LED = 0x0040 , LED connection = 0x0080.
2. Documentation Mismatch:
· Unity V2.2 and Concept V2.2, V2.6 help file uses the same byte order as table 1.
· Modicon Quantum with Unity Ethernet Network Modules User Manual (6/2006) and Transparent Ready User Guide (10/2005) use the same byte order as table 2.
We have swapped MBP_MSTR Get local statistics Word3 board status byte order when we released certain firmware versions. This also causes the product user manual, and Unity, Concept Help file board status description mismatch issue.
Considering majority users have been using the order same as the current version V3.6 for NOE77111/01 and V3.4 for NOE77100/10, we decide to remain the current MSTR board status byte order (shown in table 1) for NOE module and will make sure the consistency in our future release.
Schneider will correct the corresponding documentation to reflect the change.
Released for: Schneider Electric Saudi Arabia








Need help?
Start here!
Find answers now. Search for a solution on your own, or connect with one of our experts.
Contact Support
Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Search FAQs
Search topic-related frequently asked questions to find answers you need.
Contact Sales
Start your sales enquiry online and an expert will connect with you.