{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which Modbus function codes are supported by the TSXETG100 Modbus to Ethernet bridge?

Issue

Which Modbus function codes are supported by the TSXETG100 Mobdus to Ethernet bridge?

Product Line

ConneXium - Ethernet

Environment

TSXETG100

Resolution

TheTSXETG100 Modbus to Ethernet bridge supports all Modbus function codes. The bridge does not filter any function codes. The bridge takes the data from an Ethernet packet and sends it serially or takes the serial data and places it an Ethernet packet.

Schneider Electric Saudi Arabia