{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Runtime Error 374 Is Returned When Trying to Authorize ProWORX 32version 2.xx

Issue
Runtime Error 374 is returned when trying to authorize ProWORX 32 version 2.xx

Product Line
ProWORX 32

Environment
Windows 7

Resolution


The reason why 'Runtime Error 374' is returned when trying to authorize 'ProWORX 32' is because the current version
of 'SMTP.ocx' is incompatible with the 'ProWORX 32 version 2.xx' authorization software.

To resolve the problem,
Backup your current version
Locate the 'SMTP.ocx' file that is in your WINNT\System 32 folder..
Replace it with the attached one that is attached to this resolution, which is version 3.1.0.4.

Since this file is only needed for running the authorization software, you can replace it with the current version after the
authorization is complete.

Schneider Electric Saudi Arabia

Attachment(s)
SMTP.zip [22.57 KB]