Goals and Symptoms
- 1) Soft charge time.
- 2) Inrush current of ATV61 on power up.
- 3) Does a DC choke help limit inrush?
Causes and Fixes
- 1) The soft charge time is 1 sec maximum. It's the time to start the switching mode power supply (SMPS), and load the capacitors.
- 2) The inrush current is available for the drive up to 18,5Kw (find attached the values). Above there are no inrush current because it's a technology with thyristor so it starts like a soft starter.
- 3) Yes the DC choke limit the inrush current, in fact it decreases the dv/dt.
Legacy KB System (APS) Data: RESL181726 V1.0, Originally authored by on , Last Edited by FrCa on 01/24/2007
Related ranges: Altivar 61
Released for:Schneider Electric Saudi Arabia