Issue
The purpose of this resolution is to inform Momentum Processor and TesysU users how to wire an LULC031 to a 172JNN21032 Option Adapter via its Port 2 RS485 (RJ45 connector) for proper communications.
Product Line
Momentum
172JNN21032
Resolution
In order to communicate from the JNN Option Adapter to the LULC031 (using the XMIT or XXMIT Function Blocks), two 470-ohm biasing resistors from the + and - RS485 lines must be added and connected to a 5vdc power supply (this is required by the LULC031). When communications between the JNN and LULC031 are first initiated, it will take approximately 20 seconds for the communication parameters of the LULC031 to initialize. If the communication parameters do not change and the LULC031 was power cycled, communications will immediately be established, and no initialization is necessary. If the communication parameters are changed and the LULC031 is power cycled, initialization will re-occur for another 20 seconds to adjust to the new parameters.
120-ohm termination resistors must also be added at each end of the RS485 network.
Wiring diagram
Released for: Schneider Electric Saudi Arabia




Need help?
Start here!
Find answers now. Search for a solution on your own, or connect with one of our experts.
Contact Support
Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Search FAQs
Search topic-related frequently asked questions to find answers you need.
Contact Sales
Start your sales enquiry online and an expert will connect with you.