{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Incorrect Data Mapping of 170ADI34000 Discrete Input in 'Momentum I/O Base User Guide', part number 870USE00200

Issue
The purpose of this Resolution is to inform users of the 170ADI34000, a 16 point - 24vdc input module, that the 984LL Exec Data Mapping diagram in the Momentum IO Base User Guide is incorrect.


Product Line
Momentum
170ADI34000


Environment


Resolution
The incorrect diagram is found in the 'Momentum I/O Base User Guide', part number 870USE00200, dated 2/2007 and earlier and affects only the 170ADI34000 984LL Data Mapping diagram. It is scheduled to be corrected in a December 2007 Momentum IO Base User Guide release. The IEC Data Mapping diagram for the 170ADI34000 is correct.

This diagram shows the incorrect data mapping pinout in the User Guide


im1

This daigram shows the correct data mapping pinout.
im2


Schneider Electric Saudi Arabia