{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the serial cable to connect a Magelis XBTF terminal to an M340 PLC for Modbus communication?

Issue
What is the serial cable to connect a Magelis XBTF terminal to an M340 PLC for Modbus communication?

Product Line
Magelis XBTF

Environment
Serial Cable Modbus communication for HMI to PLC communication

Resolution
For RS-485 interface, the cable part number is XBTZ938.
The cable uses an RJ45 male connector on the M340 side and a Dsub 25-pin male connector on the XBTF side.

For RS-232C interface, there is no manufactured cable. A custom cable will need to be fabricated.

The pinout is as follows:

XBTF M340
DB25 RJ45

RxD 2 <------------------------------------------------------------> 1
TxD 3 <------------------------------------------------------------> 2
SG   7 <------------------------------------------------------------> 8

Pins 8 & 12 are jumpered                                  Pins 3 & 6 are jumpere

Schneider Electric Saudi Arabia