{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the USB cable to connect a Modicon M340 to an Magelis XBTGT2000+ series, Harmony HMIGTO, HMIG3U series?

Issue
What is the part number for the USB cable to connect a Modicon M340 to an Magelis XBTGT2000+ series, Harmony HMIGTO, HMIG2U, HMIG3U, HMIST6 series?

Product Line
Modicon M340 PLC
Magelis XBTGT
Harmony HMIGTO, HMIG2U, HMIG3U
Harmony HMIST6

Environment
HMI to PLC Modbus Communication

Resolution
Schneider Electric offers 2 different length of USB communication cables to connect a Modicon M340 to one of the above HMI families using the Modbus TCP-USB protocol:

text
USB Cable Part Number
text
Length
text
BMXXCAUSBH018
text
1.8 meter
text
BMXXCAUSBH04
text
4.5 meter

Schneider Electric Saudi Arabia