Search FAQs
Maximum torque for the connections of the time relays RE11. Maximum length that you could peel the cable ?
Goals and Symptoms
Maximum torque for the connections of the time relays RE11.
Maximum length that you could peel the cable ?
Causes and Fixes
The maximum torque for the connections of the time relays RE11 is 1Nm, screew M3 / CEI 947-1
The maximum cable peeling length for connexion is 8mm.
Legacy KB System (APS) Data: RESL192132 V1.0, Originally authored by LaBe on 06/16/2008, Last Edited by LaBe on 06/16/2008
Related ranges: Zelio Time
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: