{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a limitation of number of characters for messages displayed in the alarm banner?

Goals and Symptoms

Is there a limitation of number of characters for messages displayed in the alarm banner?

Causes and Fixes

For alarm messages, it's not documented anywhere, but the maximum length of an alarm message is 160 chars. The editor does not stop you as you add them, but it will give an error when you hit "OK" after exceeding this limit.


Legacy KB System (APS) Data: RESL192263 V1.0, Originally authored by DaBr on 07/04/2008, Last Edited by DaBr on 07/04/2008
Related ranges: Vijeo Designer

Schneider Electric Saudi Arabia