{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

'Windows Installer' error message appears after starting the 'Advantys Configuration Software'.

Issue

'Windows Installer' error message appears after starting the 'Advantys Configuration Software'.

Product Line
Advantys Configuration Software version 3.5.

Environment
Windows 7

Resolution
The new version of the 'Advantys Configuration Software' uses the new 'Windows Installer version 3.1'
which also includes newer versions of the shared ' .dll's ' written by Microsoft. Every software written
for the Microsoft Windows operatting system requires at least some of these ' .dll's '. in order to be
able to work.

The 'Windows Installer' runs as a service and is used to install software in the Microsoft Windows
operating system. It also maintains a database of the installed software and it's components.
The installing software can request that the 'Windows Installer' perform a diagnosis and repair the
program if it's component is missing or corrupted (see attached 'Overview of the Windows Installer
Technology' by Microsoft.) If the component is missing or corrupted, it will ask the 'Windows
Installer' service to repair the program as necessary by copying the files from the install source
hard drive path or CD. During the repair process, the 'Windows Installer' will display a message
requesting the install CD.



During the installation, it also checks to see if the software component is already in Windows.
If it is already installed, it checks the installed version number against the version number of the
component being installed. If the installed version is older, it overwrites it with the the newer
version and updates the 'Windows Installer' database.

After 'Advantys Configuration Software' is started, the 'Windows Installer' checks it's database to
see what '.dll's' are being shared by other installed software. When it finds that another software is
sharing a '.dll', it does a diagnosis if the other software requires it when the '.dll' is run. If the
'Windows Installer' finds something wrong it returns the 'Windows Installer' error.

The reason that the 'Windows Installer' message is appearing is because the 'Windows Installer'
found a difference during the diagnosis when it compared the version number of a shared '.dll' (used
by the 'Advantys Configuration Software') in it's database against the version number that was in
the registry setting of the other installed software.

Note: This problem is outside of Schneider Electric's control.

Attachments

(Removed File URL: 192378_62A2/Overview_of_the_Windows_Installer_Technology.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/53cf3574cadc076dc125749100529483/fl_block_5/0.58C?OpenElement&FieldElemFormat=gif)

Schneider Electric Saudi Arabia

Attachment(s)

Overview_of_the_Windows_Installer_Technology.zipOverview_of_the_Windows_Installer_Technology.zip [18.15 KB]
Explore more
Range:
EcoStruxure Control Expert (Unity Pro)
Explore more
Range:
EcoStruxure Control Expert (Unity Pro)
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.