{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can all the configuration parameters for an Advantys STB Island be written over the fieldbus via the application program?

All the configuration parameters for an Advantys STB island cannot be written over the fieldbus via the application. Some specific parameters can be written to via the RTP (Run Time Parameters) functionality. Also a memory card (SIM card) can be used to store the configuration file, then on power up, the NIM will read its configuration from the card.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: