{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

STBART0200 Firmware Upgrade to v1.62

Issue

The purpose of this resolution is to inform STB users of a firmware upgrade for the STBART0200 RTD/TC/mV module. This upgrade addresses the issue where in extreme rare instances the module would display a blinking ERR LED and both input readings would be zero. At that time 0x81 was displayed in a channel Status Register.
A/D Converter fault states resulting from exposure to EMI levels far greater than those defined by test standard EN61131-2 have been overcome by implementing a retry mechanism in the modules firmware.

Product Line
Advantys,STB

Resolution

1. Hot swap of the affected module restored it's operation.
2. STBART0200 firmware is not field upgradeable.
3. Modules with the new firmware are labeled:

SV:01.62
PV:07

Schneider Electric Saudi Arabia

Explore more
Range:
Modicon STB
Explore more
Range:
Modicon STB
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.