{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What kind of application is this relay RM35S0MW built for? How to use it ? Is there some limitation?

Goals and Symptoms

What kind of application is this relay RM35S0MW built for?
How to use it ?
Is there some limitation?

Facts and Changes

RM35S0MW

Causes and Fixes

Speed Measurement and Control Relay

The relay counts the time between each pulse and evaluates the speed.
This value is compared with the preset value to determine whether if the system is under or over speed. The pulse interval can vary from 0.05 seconds to 10 minutes

The main application are escalators, monitoring of rotation speed, transporter or conveyor belt speed, pump rotation, industry process systems..

Interval between pulses (measurement range) corresponds to frequency (Hz) and speed (rpm):
Time Frequency (Hz) Frequency (rpm)
0.05 to 0.5s 2 to 20 120 to 1200
0.1 to 1s 1 to 10 60 to 600
0.5 to 5s 0.2 to 2 12 to 120
1 to 10s 0.1 to 1 60 to 6
0.1 to 1 mn 0.017 to 0.178 1 to 6
0.5 to 5 mn 0.033 to 0.33 0.2 to 2
1 to 10 mn 0.0017 to 0.017 0.1 to 1
A relay can only control one characteristic: Undervoltage or Overvoltage.
You cannot do both. On the other hand, you must use 2 relays and select it with the knob N°1. Then you select the range (Knob N°3) and adjust % (Knob N°2) according to the speed to control.

Example :
A speed 900rpm corresponds to 15Hz(900/60) and then to a time of 0.067s. You select with the knob N°3 the time range 0.05 to 0.5s and the select 13.33% with knob N°2

Currently, we do not have another relay that control a speed higher than 1200rpm.
If you have a speed higher, you can use a reduction gear


Legacy KB System (APS) Data: RESL197713 V1.0, Originally authored by BrCa on 09/02/2009, Last Edited by BrCa on 09/02/2009
Related ranges: Zelio Control

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: