{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
When a phase is connected to neutral ( N ) terminal, is the RM35UB3N30 protected against this ? If so, how would the unit react on this fault.

Goals and Symptoms

When a phase is connected to neutral ( N ) terminal, is the RM35UB3N30 protected against this ? If so, how would the unit react on this fault.

Facts and Changes

RM35UB3N30 RM35U
Wrong connection
Phase
Neutral

Causes and Fixes

If there is a error in connecting the product , and a phase is connected to the neutral ("N" terminal), there is a risk of destruction.


Legacy KB System (APS) Data: RESL197893 V1.0, Originally authored by LaBe on 02/26/2009, Last Edited by LaBe on 02/26/2009
Related ranges: Zelio Control

Schneider Electric Saudi Arabia