{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I setup Vijeo Citect V7.0 for redundant LAN?

Goals and Symptoms

The purpose of this resolution is to provide a solution for LAN redundancy with Vijeo Citect V7.0

Causes and Fixes

This requires two NIC cards in the Vijeo Citect server PC. It is recommended to run the ethernet cable to a different path (conduit) to another ethernet switch. So that in the event of a link or ethernet switch failure, the other path may still provide data to the Vijeo Citect I/O Server.Citect Project Editor - Redundant LAN

Schneider Electric Saudi Arabia