{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Cannot download to the STBNIP221 after updating to version 2.71

Issue
Cannot download to theSTBNIP221 after updating to version 2.71

Product Line
STBNIP2212

Environment
Windows 7

Resolution

This could happen if the application was created in an older version of the Advantys Configuration Software
and that same version is being used to perform the download.

To resolve the problem:

  • Update to the latest version of the Advantys Configuration Software.
  • Open the project.
  • Click on 'File\Save' to save the project.

Schneider Electric Saudi Arabia