{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What does it mean the "socket operating voltage" expression of the RSL slim interface relay? The catalog has a table which describe the operating vol...

Goals and Symptoms

What does it mean the "socket operating voltage" expression of the RSL slim interface relay?
The catalog has a table which describe the operating voltage and the control circuit voltage for each sockets. What is it?

Facts and Changes

socket operating voltage of RSL relay

Causes and Fixes

First, depending on the 4 types of slim-relays (input voltages: 12, 24, 48, 60 Vdc), there are 6 types of sockets.
Therefore, the 6 sockets have to be controled with special voltages which is indicated as the "operating voltage" : 12, 24, 48, 60, 110, 230 Vac/dc.

The Operating voltage column indicates the voltage to activate the relay.
The Tolerance column indicates the mini/maxi of the Operating voltage.
The Control circuit voltage column indicates the voltage which will be applied on the input of relay (in order to indicate to the customer the right voltage rating of relay, if he replaces it).

The Output ratings are indicated in "contact characteristics" and "socket characteristics".


Legacy KB System (APS) Data: RESL201321 V1.0, Originally authored by LaBe on 02/24/2010, Last Edited by LaBe on 02/24/2010
Related ranges: Zelio Relay

Schneider Electric Saudi Arabia

Explore more
Range:
Zelio Logic SR2/SR3
Explore more
Range:
Zelio Logic SR2/SR3
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.