Goals and Symptoms
Problem with SIS Label software V3.2U
Facts and Changes
SISLABEL
XBY2U
Causes and Fixes
SIS Label software version 3.2U contains two malfunctions:
1/ WYSIWYG function:
When a new label model containing text is created, or when text is added to an existing model, text printing differs from its appearance on the screen.
2/ Text selection:
When text is selected in a label model it can be modified, but no information is displayed in the "character size" field. If entry of new text is required, a value must first be selected in the "size" field in order to activate the "insert text" button
To correct these two malfunctions, 5 patches have been created, each of which corresponds to an of SIS Label 3.2U (XBY2U) installation language:
Sislabel_French_01.exe
Sislabel_English_01.exe
Sislabel_German_01.exe
Sislabel_Italian_01.exe
Sislabel_Spanish_01.exe
By default the patch is installed in the SIS Label installation directory:
C:\Program Files\Schneider Electric\SISLabel
The customer can of course select an alternative installation path.
Please find below the link for patch downloading:
Legacy KB System (APS) Data: RESL202275 V1.0, Originally authored by LaBe on 05/17/2010, Last Edited by LaBe on 05/17/2010
Related ranges: Harmony XB4