Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
How do I setup serial communication between a Twido and a Magelis HMISTU655 using TwidoSoft v3.5?

Goals and Symptoms

This resolution provides a solution for setting serial communication between a Magelis HMISTU655 and a Twido. The RS485 port 1 and port 2 will be used on the Twido to communicate to a HMISTU655 HMI.

 

Causes and Fixes


Hardware:
TWDLCDA24DRF : Twido Compact PLC
TWDNAC485D: RS 485 connection module for Compact base
HMISTU655: Magelis HMI 3.5"

XBTZ9780 cable: Serial communication cable:
(or XBTZ978 + XBTZN999 adapter)

Software:
Twidosoft v3.5
Vijeo Designer v5.1

 

1) Setup the Twido Port 1 with the following parameters:
Type: Modbus
Address: 1
Baudrate: 19200
Data Bits: 8 (RTU)
Parity: None
Stop Bits: 1
Response Timeout: 10
Inter-frame delay: 10

Comm

Note: Parity must be set to None on Port 1.

 

2) Configure the TWDNAC485 optional port.
port

 

3) Setup the Twido Port 2 TWDNAC485 with the following parameters:
Type: Modbus
Address: 1
Baudrate: 19200
Data Bits: 8 (RTU)
Parity: None
Stop Bits: 1
Response Timeout: 10
Inter-frame delay: 10

comms

Note: Parity can be set to None or Even on Port 2 using the TWDNAC485D.

 

4) Create the following Ladder section.

comms

This initialize the memory words so that the TWIDO can communication to the HMISTU655. In a real application this may not be required.

 

5) In Vijeo Designer, configure the Modbus RTU serial driver with the following parameters:

Serial Interface: RS485
Transmission Speed: 19200
Retry Count: 2
Parity Bit: None
Stop Bit: 1
Rcv. Time Out: 1 (Sec)
TX Wait Time: 10 (Msec)
config

 

6) In Vijeo Designer, configure the Modbus EQUIPMENT with the following parameters:

Slave EQUIPMENT Address: 1
Preferred Frame Length: Custom, 120 bytes
IEC61131: 0-based
Word Order: High Word First
ASCII Display: Low byte first
config

 

7) Create a Integer variable link to %MW10 in Vijeo Designer
variables

 

8) Add a Numeric Display field and configure as shown below:
settings

Attachments

(Removed File URL: 202708_F0BE/HMISTU655.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/441585c9b16dbd42c125774b0010cccf/fl_block_5/0.544?OpenElement&FieldElemFormat=gif)(Removed File URL: 202708_F0BE/Twido.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/441585c9b16dbd42c125774b0010cccf/fl_block_5/0.1116?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL202708 V1.0, Originally authored by MiMe on 06/23/2010, Last Edited by MiMe on 06/23/2010
Related ranges: Twido

Schneider Electric Saudi Arabia

Attachment(s)
Twido.zip [2.38 KB]
HMISTU655.zip [8.47 KB]