{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does Schneider offer a conversion tool which will allow me to migrate 800 Series I/O to Quantum, without rewiring my I/O?

Yes. Please see attached PDF file. 800_to_Quantum.pdf


Note: The Quantum seried will be obsoleted 12/31/2018 and the new upgrade option for the 800 series will be the M580 with the X80 I/O and that also has conversion kit to go from 800 to x80.


Rev 7/7/2017

Schneider Electric Saudi Arabia