{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do K1S... , K2S.... cam switches conform to ROHS and REACH standard?

Goals and Symptoms

Do K1S... , K2S.... cam switches conform to ROHS and REACH standard?

Causes and Fixes

We cannot provide a ROHS and REACH certificates for each specific cam switch. These products are ordered with generic references K1S, K2S. So they are not included in standard commercial list for approval, this is why it is not possible to check them on Planet.
However, they are using same parts as standard product, so they are compliant with RoHS.
For ROHS and REACH certificates, you have to interrogate Planet with the generic reference K1S or K2S which are covering all specific range.
https://checkaproduct.se.com/CheckProduct.aspx?cskey=a61392e5f18945f598df1443aa95df6c

Schneider Electric Saudi Arabia