{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Wiring a TCSESM ConneXium switch power plug for use without redundant power source.

Goals and Symptoms

Wiring a TCSESM ConneXium switch power plug for use without redundant power source.

Causes and Fixes

The ConneXium TCSESM managed switch line supports redundant power supplies. If you are not using a redundant supplies and the fault light is on then all you need to do is jumper the two power inputs together. This will turn the fault light off. If this does not eliminate the fault light refer to the Quick Reference Guide for the product.


Schneider Electric Saudi Arabia