{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Do I have to convert my Concept 2.5 project to Concept 2.6?

Article available in these languages: Spanish

Applications created with Concept 2.5 SR2 or later are directly compatible with Concept 2.6 SR1 or later.
No program conversion is necessary.
Applications created with older versions of Concept (V1.x or V2.x) can be maintained under Concept 2.6 SR1 or later after being
converted using the included Concept Converter tool.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: