Goals and Symptoms
Quantum 140NOE77101 ethernet module firmware v5.0 upgrade procedure using the Unity OS Loader tool…
Causes and Fixes
Purpose
To outline the steps required to upgrade a NOE module using Unity Pro 2.2 or higher OS loader. Please note that prior version of the OS loader are not compatible with this revision of the firmware. You MUST be at the proper OS loader revision of 2.2 or higher.
Applicable Modules
140NOE77101 Kernel 2.0 or higher with a minimum of V4.2 Firmware.
Resulting Module after upgrade
140NOE77101 Kernel 2.0 or higher, Firmware V6.8
Overview
The upgrade of a NOE module requires multiple steps. Two components must be considered to be upgraded, the Kernel and the Firmware version. Not all steps listed below may be required depending on the version of the NOE module before this upgrade procedure is started.
Pre-conditions
The CPU module must be in STOP mode and the NOE must have NO TCP traffic.
A loss of power during the upgrade may cause the NOE module to be inoperable. Make sure the power supply on the NOE module rack will not be interrupted during the upgrade.
Step 1
Verify the Kernel and Firmware using Unity OS loader or NOE web page.
For modules that have Kernel V1.0 and Firmware Lower than V3.3, you must upgrade to Kernel V2.0 and Firmware V3.30 before continuing with upgrade.
For modules that have Kernel V2.0 or higher and Firmware V4.2 or higher, you may continue upgrading to Firmware V6.8 using the Unity OS loader V2.2 or higher.
Step 2
Open the Unity OS loader tool.
Step 3
Select the FTP Driver.
Select Next.
Step 4
Select Direct Device and enter the device IP address and select Connect. If requested enter the modules MAC address, the MAC address can be found on the front of the module.
Note: If your module is located remotely, you can get the MAC address by pinging the module's IP address, then using the arp-a command to display the module's physical MAC address.
Select Next.
In this example, the IP address used is 192.168.30.13. Adapt this address for the one of your PLC.
Step 5
Select Operation Download OS to Device
Select Browse and then select the correct 140NOE77101 file to download.
If module is listed select the correct file and click Next.
Step 6
The following Screens will appear:
Both the Hardware ID and OS version must be followed by a green tick.
Select Next and then Download.
If this screen does not appear recheck each step and contact your local Schneider office for assistance if required.
Select Close and Back in the OS loader.
Exit the OS loader.
Allow the module 60 seconds to complete any actions and power cycle the module to allow the new Firmware to be loaded.
NOE77101 Web Server properties page screen shot on completion of upgrade.
Released for:Schneider Electric Saudi Arabia