Search FAQs
Implementing CIP Explicite messaging to Modbus object between a 140NOC78000 (client) and a 140NOC78000 (server)
Issue
When using the 140NOC78000 as a server, to get process data through the Modbus object, only Unconnected_ Send messaging will work. The attachment is an example on how to perform an Explicit messaging using the MBP_MSTR block from a 140NOC78000 client.
Product Line
Quantum
140NOC78000
Environment
Resolution
Using UCMM and connected messaging will only return diagnostic data when communicating to a 140NOC78000
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: