{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
BMXNOC0401 Explicit Messaging CIP Modbus Object Write Example

Issue
The attached document is a CIP Modbus Object Write example for a BMXNOC0401 using the DATA_EXCH block to write to a Quantum 140NOC77101.


Product Line
M340
BMXNOC0401


Environment


Resolution
This program will write to located registers in Schneider PLC's with the following network modules installed:

  • 140NOC77101
  • BMXNOC0401
  • TSXETC101

Do not use this example to write located registers in Schneider PLC's through the following network module:
  • 140NOC78000

Schneider Electric Saudi Arabia

Attachment(s)
BMXNOC0401_CIP_Modbus_Object_WRITE_Example.pdf [199.08 KB]