{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to recover when the HART DTM is interrupted when the STBNIP2311 goes to fallback mode?

Issue
If the STB Island goes into a fallback state, communication through HART DTMs will be interrupted.
Error messages for connected DTMs will be displayed in Unity Pro and AMS applications.



Product Line
STB HART


Resolution
When the STB Island recovers from the fallback state, the user must reconnect all connected HART DTMs.


Legacy KB System (APS) Data: RESL210501 V1.0, Originally authored by DaDz on 02/01/2013, Last Edited by DaDz on 02/01/2013
Related ranges: Modicon STB

Schneider Electric Saudi Arabia