{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Control Expert (formerly Unity Pro) is generating a "Task Overrun" error which sets %S19 . What is the most likely cause of this error?

The Task Overrun error (%S19) is set to 1 when the time it takes to complete a Task exceeds the specified time.
The MAST & FAST Task's use the WDT setting to determine when %S19 will set. The user must reset this bit to 0.

Note : If this happens repeatedly, the program may be need to be reviewed. For instance, the program may have for loop in a ST section that does not exit the loop properly and that could cause a watchdog over run. If it is not the program then the Hardware needs to be set for a TEX.

Schneider Electric Saudi Arabia