{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can I monitor IO module health in an M340 application?

Issue
Looking for a way to monitor the general overall heath of an IO module in the backplane.

Product line
Modicon 340, Modicon X80, Control Expert, Unity Pro

Resolution
Yes, you can monitor the health of an IO module. Unity offers %SW160 - %SW163 for this purpose.
Each bit within the word will represent a module location along the bus. For example %SW160.3
would contain the health status of rack 0, slot 3. If the bit value is "1" the module is healthy, if the bit value is "0" the module is unhealthy. Each of the remaining %SW's in this group of 4 represent
expansion backplanes.



Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: