Cold Start = going from Unconfigured to Configured.
If you Transfer a project to an M340 that has a configuration with State Ram, Scenario 2 will leave existing state ram data unchanged.
If you power up an M340 with no SD card and then insert the SD card, Scenario 2 leave all data at 0.
- When checked, those %MW 's with initial values will be loaded. Any %MW not having an initial value will be cleared (initialized) to 0.
- If unchecked the all %MW's are cleared to 0 regardless of the presence of initial values.
- Unlocated variable values are maintained regardless of whether this box is checked or unchecked.