{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I troubleshoot a copper Modbus Plus network physical installation?

Issue:
There is no communication on my Modbus Plus network. How can I troubleshoot the lines to make sure I do not have a connection problem or another issue with the cabling?

Product Line:
Quantum PLC
Premium PLC
Momentum PLC

Environment:
EcoStruxure Control Expert (Formerly Unity Pro)
Concept
ProWorx

Resolution:
The following are some basic troubleshooting tips to check a copper MB+ physical network installation. Good cabling practices should always also be employed in routing and installing MB+ cabling:

1Ensure only Modicon cabling and cabling components are used.
2Ensure no two adjacent nodes have less than 10 ft of physical cable between them (except if using Momentum product with cluster mode components).
3Ensure there are no splices.
4Ensure the topology is purely linear (branching is not allowed).
5Ensure taps are properly sided left-to-right, left-to right. (The grounding lug on the standard taps can be utilized to determine proper siding).
6Ensure all nodes are properly grounded.
7Ensure no more than 32 nodes exist on the network without a RR85 repeater (usage of a RR-85 repeater allows up to 64 nodes max on the network).
8Ensure the total network length does not exceed 1500 ft without usage of a RR-85 repeater (3 RR-85 repeaters can be utilized to connect up to 4 segments to make a total maximum network length of 6000'.
9Check the resistance of the MB+ network. Disconnect all nodes from the network then measure resistance between the white and blue leads at any point. The resistance should be approx. 60 Ohms (derived from two 120 Ohm resistors in parallel). While spec is 60-80 Ohms, If 68 or more Ohms is read, then check the network for loose connections or damaged ferules on taps. Read resistance directly across a tap to check for resistance. Virtual continuity should be read. If more than negligible resistance is read, reseat connections. If this does not reduce resistance, replace the suspect connector or tap. If 120 Ohms of resistance is read, check cable for a break or loss of end termination at either side of the network.

Schneider Electric Saudi Arabia