{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the two types of displays that can be used with CM4000 and do they come with a cable to connect to the meter?

Issue
What are the two types of displays that can be used with CM4000 and do they come with a cable to connect to the meter?

Product Line
CM4250, CM4000T, CM4000

Cause
Customer wants to know the options for ordering the display for CM4000 series meter.

Resolution
The two options for display are shown below with their respective part number and description:

CMDLC: Liquid Crystal Display W/Bk. Ltg.- 4line x 20 character (Newer one)
CMDVF: Vacuum Fluorescent Display- 4 line x 20 character

Both the CMDLC and CMDVF includes a 12 foot communication cable (CAB12) that can connect to the CM4000 meter.


Schneider Electric Saudi Arabia